|
Connectivity |
|
Single Connection Saves Time and Money with STN Panels
The RJ12 modular connector on the STN panels (both 3" and 6") is a serial port which can also supply 5VDC power to the units. It can be used for programming, PLC communication, and power.
The 6" STN model also includes a DSUB15 serial port, which can be configured for RS232, RS422, or RS485. The 6" units also have a separate connection for 24 VDC built-in.
When using most AutomationDirect (Koyo) PLCs with a 6 pin Modular RJ12 type connector - no additional power adapter is required - saving you time and money. Some other protocols are also supported.
DC power adapters are also available for the 3" panels.
TFT Panels have USB Ports & Serial
Step-up to either the 4" TFT Panel or the 6" model for a standard "type B" USB programming port. The USB port even supplies power to the panel during programming so you don't have to bother hooking up 24 VDC during programming operations
|
![]() |
||
|
Note: See the C-more Micro-Graphic Hardware User Manuals (P/N: EA1-MG6-USER-M or EA1-TCL-M), Chapter 6: PLC Communications, for wiring
diagrams that the user can use to construct their own cables.
Note: For EA1-S6ML and EA1-S6MLW; some PLCs can provide 5 VDC power through the DV-1000 serial cable, and no external 12-24 VDC souce is required. However, screen
brightness is diminished and the alarm beep will not function. This Low-Power Mode should be used during initial programming and check-out only. Connect
an external 12-24 VDC power source when the panel is installed in its application. EA1-T4CL and EA1-T6CL do not offer Low Power Mode, and require an external power
supply.
|
|||
Programming Connection |
||
![]() |
$Call
Part # EA-MG-PGM-CBL |
|
The USB to RS-232 programming cable assembly and adapter is used to program the C-more Micro STN units via the RJ12 modular connection and also supplies 5VDC power to the C-more Micro panel during the programming process. The TFT units use a standard USB A-to-B type cable(such as USB-CBL-AB6)for programming. |
||
PLC Drivers for C-more Micro
The following protocols are supported, and all the drivers are included with C-more Micro:
• AutomationDirect CLICK
• AutomationDirect DirectLogic K-sequence
• AutomationDirect DirectLogic DirectNet
• AutomationDirect DirectLogic Modbus
• Entivity (Think&Do ) Modbus
• Modbus RTU
• Allen Bradley DF1 Full Duplex
• Allen Bradley DF1 Half Duplex
• Allen Bradley PLC5 DF1
• Allen Bradley DH485
• GE Fanuc 90/30 SNPX
• Mitsubishi Melsec FX
• Mitsubishi Q and QnA Series
• Omron Host Link Adaptor
• Omron CS/CJ Series FINS
• Siemens PPI
Our larger C-more panels offer additional driver options. |
||
|
PLC Cables for C-more Micro
The DV-1000 serial cable connects the C-more Micro RJ12 connection to most
AutomationDirect DirectLogic PLCs. The D4-1000 cable is used for the DL405 PLC. Specific cables are available for most of the supported PLCs and protocols.
• Here is the complete connectivity chart for the 3" panels.
• A separate connectivity chart is supplied for the 4" and 6" (both STN and TFT) panels.
|
|
Other Options for Powering & Connecting to C-more Micro 3" STN Panels
When connecting C-more Micro 3" units to other brands of PLCs, a 12-24VDC power adapter must be installed. Two versions are available
• The EA-MG-P1 allows C-more Micro 3" to be powered from a separate 12-24VDC power source (more)
• The EA-MG-SP1 also allows the use of 12-24VDC power and offers a second serial port (DB-15 style) for 3" units (more)
Neither of these option modules is needed (nor can they be used) with C-more Micro 4" or 6" units . Those units already offer externally powered operation, and they have the serial port (DB-15 style) built-in.
|
|||
![]() $Call
12-24 VDC power adapter (use if your PLC doesn't supply 5V) - more
Part # EA-MG-P1 |
![]() $Call
12-24 VDC power adapter and a second serial port (DB-15) - more
Part # EA-MG-SP1
|
||